SWRU368C May 2018 – January 2021 CC3100 , CC3100MOD , CC3200 , CC3200MOD
Open a serial connection application like TeraTerm or Putty (any other terminal emulator program can be used), and configure the settings:
Parameter | Value |
---|---|
Baud Rate | 921600 |
Data Bits | 8 |
Stop Bits | 1 |
Parity | None |
Flow Control | None |
If you are using a CC31XXEMUBOOST, connect the fourth port in Device Manager.
Configure the terminal emulation to work in binary mode (and not textual/ASCII mode) and record the log. Here are some examples:
Tera Term
Setup → Serial Port…
File → Log...
Putty
On the left side of the screen, select Connection → Serial:
In the menu screen before connecting to the port: