To stop the SmartConfig operation call:
sl_WlanSmartConfigStop()
Note: - After the device is connected to the requested network it should receive an IP address from the AP or router.
- The SmartConfig operation may not end successfully if the Wi-Fi network to which the smart phone is connected uses transmissions modes and rates not suitable for SmartConfig. In this case, use the AP Provisioning method.