SWRU368C May 2018 – January 2021 CC3100 , CC3100MOD , CC3200 , CC3200MOD
The device is a P2P client by automatic connection, using fast connection after each reset or disconnection. The device stores the parameters of the last connection.
At least one profile should be configured in the system.
On fast connect, add the device to P2P supplicant to avoid find.
Send P2P-Invite to remote persistent GO with network parameters.
If fast connection failed, fall back to profile P2P find and perform the regular connection method (join or full negotiation).