SWRU368C May 2018 – January 2021 CC3100 , CC3100MOD , CC3200 , CC3200MOD
The mDNS service in the Simplelink implementation is started by default with the following names:
The target name is the name that should be in ‘A’ query (query for getting the IPv4). The name is assembled from the MAC address of the target, the word “mysimplelink”, and the domain of the local network. The user can change this name by setting the URN name or by a smart-configure operation.