The user can open one transceiver socket in the system.
The length of a received packet will be trimmed if it exceeds 1472 bytes.
Cannot transmit frame over 1472 bytes and below 14 bytes.
If using the SimpleLink studio, note that the maximum throughput of the SPI is 5~6Mbps, so in a crowded WIFI medium, there will be packet loss.
The transceiver will not open in connection or connected mode. Notice that auto connection mode is also considered as connected mode, even if not connected.