SWRU368C May 2018 – January 2021 CC3100 , CC3100MOD , CC3200 , CC3200MOD
Wi-Fi provisioning is the process of connecting a new Wi-Fi device (station) to a Wi-Fi network (access point). The provisioning process involves loading the station with the network name (often referred to as SSID) and its security credentials. The Wi-Fi security standard distinguishes between personal security, mostly used in homes and businesses, and enterprise security, used in large offices and campuses. Provisioning a station for enterprise security usually involves installing certificates, which are used to verify the integrity of the station and the network by interaction with a security server managed by the IT department. Personal Wi-Fi security, on the other hand, needs to be handled by users at home, and it simply involves typing a pre-defined password. To provide robust security, the password can be as long as 64 characters.
For more details on provisioning code example and usage, see the simplelink wiki: http://processors.wiki.ti.com/index.php/CC31xx_%26_CC32xx_Provisioning_Features.