SWRU368C May 2018 – January 2021 CC3100 , CC3100MOD , CC3200 , CC3200MOD
To start SmartConfig manually, send the following command:
sl_WlanSmartConfigStart(groupIdBitmask,
cipher,
publicKeyLen,
group1KeyLen,
group2KeyLen,
publicKey,
group1Key,
group2Key)
Parameters description:
To encrypt the password when the encryption key is not stored in the serial flash of the device, use:
To encrypt the password when the encryption key is stored in the serial flash of the device, use:
To avoid encrypting the password use:
After sending this command, SmartConfig starts.
When running SmartConfig manually, if a key to encrypt the password is stored in the external serial flash or supplied at the command, this key must be supplied in the SmartConfig application.