SWRU368C May 2018 – January 2021 CC3100 , CC3100MOD , CC3200 , CC3200MOD
When in AP mode, access to the web page is performed using the domain name. The domain name is configured with the host API.
In AP mode, the SimpleLink is also accessed using the IP address.
The default domain name is mysimplelink.net.
Accessing the web page can be performed with either mysimplelink.net or www.mysimplelink.net.
Using the www. prefix in the domain name when the domain name does not match, the server internally removes this prefix and tries to search without it.
Use the www. prefix in the domain name search because commercial browsers behave better from a DNS perspective.