SWRU372C June 2014 – March 2020 CC3200
To measure the current draw of the CC3200, use the 3V3 jumper on the jumper isolation block (J12). The current measured in this mode includes only the CC3200 current and no external blocks. However, if a GPIO of the CC3200 is driving a high current load like LED, then that is also included in this measurement.