This document provides detailed information about various WiLink 8 and Wi-Fi® features, as well as TI proprietary enhancements. The document does not provide the complete application programming interface (API) set, but a high-level overview of the features. The WiLink 8 Linux® software package (NLCP) is based on the open source mac802.11 implementation; the complete API can be found in: http://lxr.free-electrons.com/source/net/mac80211/.
WiLink is a trademark of Texas Instruments.
Bluetooth is a registered trademark of Bluetooth SIG, Inc.
Linux is a registered trademark of Linus Torvalds.
Wi-Fi is a registered trademark of Wi-Fi Alliance.
All other trademarks are the property of their respective owners.