SWRU423A July 2015 – May 2016 WL1801MOD , WL1805MOD , WL1807MOD , WL1831MOD , WL1835MOD , WL1837MOD
In this mode, the STA remains in sleep mode most of the time, even during intervals of receiving traffic.
The AP buffers the data destined to the STA in forced power-save mode and publicizes in its beacon that it has data for the specific associated station. The STA is awakened by the predefined interval and detected in the beacon of the AP if there is any data for the station in the AP’s buffer.
When saved data is in the buffer, the STA sends a trigger packet that pulls the data from the AP. In the data packets, the AP enables the bit that indicates “more data”, which lets the STA know it should stay awake for more packets until it receives a frame from the access point indicating “no more data”. The STA then returns to sleep and this cycle repeats itself.