The SimpleLink™ Wi-Fi® SensorTag from Texas Instruments™ (model CC3200SensorTag) provides a demo platform for showcasing the capabilities of the CC3200 device. With this easy-to-use platform, environmental sensing and other Internet of Things (IoT) applications can be done with ease.
The CC3200 device is part of the SimpleLink microcontroller (MCU) platform which consists of Wi-Fi®, Bluetooth® low energy, Sub-1 GHz and host MCUs. All share a common, easy-to-use development environment with a single core software development kit (SDK) and rich tool set. A one-time integration of the SimpleLink platform lets you add any combination of devices from the portfolio into your design. The ultimate goal of the SimpleLink platform is to achieve 100 percent code reuse when your design requirements change. For more information, visit www.ti.com/simplelink.
Texas Instruments, SimpleLink, Internet-on-a chip, LaunchPad are trademarks of Texas Instruments.
ARM, Cortex are registered trademarks of ARM Limited.
Apple is a registered trademark of Apple, Inc.
Bluetooth is a registered trademark of Bluetooth SIG, Inc.
IOS is a registered trademark of Cisco Systems, Inc.
Google Play is a trademark of Google.
IBM is a registered trademark of IBM Corporation.
Wi-Fi is a registered trademark of Wi-Fi Alliance.
All other trademarks are the property of their respective owners.
The high-performance CC3200 device is the industry's first single-chip microcontroller (MCU) with built-in Wi-Fi connectivity for easy system application. Created for the Internet of Things (IoT), the SimpleLink™ Wi-Fi CC3200 device is a wireless MCU that integrates a high-performance ARM®Cortex®-M4 MCU that allows customers to develop an entire application with a single device. With on-chip Wi-Fi, internet, and robust security protocols, no prior Wi-Fi experience is needed for fast development.
The CC3200 SensorTag is a low-cost IoT demo platform for ARM® Cortex®-M4F-based microcontrollers. The SensorTag design highlights the CC3200Internet-on-a chip™ solution and Wi-Fi capabilities. The CC3200 SensorTag features programmable user buttons, LEDs, reed relay, digital microphone, and a buzzer for user interaction. Onboard sensors, gyroscope, accelerometer, and compass allow for easy environmental sensing and IoT applications. Figure 1 shows the CC3200 SensorTag.
NOTE
All figures and references in this document apply to the Rev1.2. Most of the text in this document also applies to the Rev1.2, unless otherwise stated.
CAUTION
The kit contains electrostatic discharge (ESD) sensitive components.
Handle with care to prevent permanent damage.