SWRU546E October 2018 – May 2022 AWR6843 , AWR6843AOP , IWR6443 , IWR6843 , IWR6843AOP
When used in Modular mode, the UART can either be routed to the CP2105 device, which displays the data on the mmWave visualizer, or to other devices connected to the USB interface. The UART data can also be routed to the CC2642R2F, which transmits data to a wireless device through Bluetooth. Figure 4-12 shows the setup for CP2105. Figure 4-13 shows the setup for CC2642R2F. (1)