SWRU548C February 2019 – September 2021 CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF
A compatible BoosterPack module can be stacked on top of the LaunchPad kit using the two 20-pin connectors. The connectors do not have a key to prevent the misalignment of the pins or reverse connection. Ensure that the VCC and 5-V pins are aligned with the BoosterPack header pins. On the CC3235MODSF LaunchPad kit, a small white symbol is provided near pin 1 (see Figure 4-1) to orient all BoosterPack modules.