SWRU548C February 2019 – September 2021 CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF
The RF signal from the module is routed to the antenna using a coplanar waveguide with ground (CPW-G) structure. CPW-G structure offers the maximum amount of isolation and the best possible shielding to the RF lines. In addition to the ground on the L1 layer, placing GND vias along the line also provides additional shielding. Figure 3-7 shows a cross section of the coplanar waveguide with the critical dimensions.
Figure 3-8 shows the top view of the coplanar waveguide with GND and via stitching.
The recommended values for the PCB are provided for 2-layer boards in Table 3-2 and for 4-layer boards in Table 3-3.
PARAMETER | VALUE | UNIT |
---|---|---|
W | 26 | mils |
S | 5.5 | mils |
H | 42.1 | mils |
Er (FR-4 substrate) | 4.2 | F/m |
PARAMETER | VALUE | UNITS |
---|---|---|
W | 21 | mils |
S | 10 | mils |
H | 16 | mils |
Er (FR-4 substrate) | 4.5 | F/m |