The CC3235MODSF LaunchPad development kit's Out-of-Box Experience (OOBE) demonstrates and highlights the following features:
- Easy connection to the CC3235MODSF LaunchPad:
- Using the SimpleLinkTM Wi-Fi® Starter Pro application (available on iOS and Android™), users can use Access Point (AP) provisioning or SmartConfig™ provisioning for a fast CC3235MOD connection.
- Configuring the device in AP mode gives users a direct connection to the CC3235MODSF LaunchPad.
Once the device is provisioned and connected to an AP in station mode, the profile is stored on the local file system so that any reset to the CC3235MODSF automatically connects it to the AP.
- Easy access to the CC3235MODSF through its internal web server, using either:
- The SimpleLinkTM Wi-Fi® Starter Pro application
- Any browser; web pages stored on the serial flash are loaded on the browser, to provide ease of use.
This feature demonstrates configuring and reading onboard sensors.
- Over-The-Air (OTA) updates that demonstrate an update of a full image. OTA service enables in-system updates of the MCU application, CC3235 firmware releases (Service Pack) made available by TI, and other vendor files. An update procedure executed in a full-system integrity fashion, such as failure to upgrade any image components, results in rolling back to the previous valid version.
Visit the CC3235 LaunchPad Out-of-Box Experience Guide on
SimpleLink Academy (see Section 6.3) for more details.