SWRU561A September 2020 – October 2020 WL1801MOD , WL1805MOD , WL1807MOD , WL1831 , WL1831MOD , WL1835MOD , WL1837MOD
This demo shows how to use the WiLink device as both a station and as an AP, using the out-of-box scripts available at /usr/share/wl18xx. An example use-case for a multirole Wi-Fi device might be to act as a wireless bridge. In multirole, the WiLink device can connect to an internet-enabled secure AP (STA mode) as a client, while simultaneously acting as a station to which other devices can then connect to for internet access. The same hardware used for AP mode testing can be used.