SWRU576 January   2021 WL1801MOD , WL1805MOD , WL1807MOD , WL1831MOD , WL1835MOD , WL1837MOD

 

  1.   Trademarks
  2. Introduction
    1. 1.1 Acronyms Used in This Document
  3. Peer to Peer (P2P) Mode
    1. 2.1 P2P Device
      1. 2.1.1 Searching Phase
      2. 2.1.2 Negotiation
      3. 2.1.3 Group Formation
    2. 2.2 PSP Client
    3. 2.3 P2P GO
    4. 2.4 P2P Commands
      1. 2.4.1 P2P Commands Detailed Information
        1. 2.4.1.1 p2p_find
        2. 2.4.1.2 p2p_connect
        3. 2.4.1.3 p2p_listen
        4. 2.4.1.4 p2p_group_add
        5. 2.4.1.5 p2p_group_remove
        6. 2.4.1.6 p2p_peer
        7. 2.4.1.7 p2p_invite
      2. 2.4.2 P2P Event Details
    5. 2.5 P2P Use Cases
      1. 2.5.1 P2P Connection in PBC (Push Button Control)
      2. 2.5.2 Create Autonomous 1:2 P2P Group (Push button Control)
        1. 2.5.2.1 Assigning IP Address in P2P Mode Using DHCP Method
        2. 2.5.2.2 Create 1:2 P2P Group - Connect With PIN Code
        3. 2.5.2.3 P2P Invitation Procedure - Create Autonomous 1:2 P2P Group, (Push button Control)
  4. Access Point (AP) and Peer-to-Peer (P2P) Multirole
    1. 3.1 Errata/Limitations
  5. Multi BSSID (mBSSID)
    1. 4.1 Setup and Configuration
    2. 4.2 User Guide and Examples
  6. Access Point (AP) Enhanced Low Power (ELP) Mode
    1. 5.1 Setup and Configuration
    2. 5.2 User Guide and Examples
    3. 5.3 Errata/Limitations
  7. WiLink8 Wake on WLAN (WoWLAN) Feature
    1. 6.1 Mode of Operation
    2. 6.2 Adding "Suspend/Resume" WoW Mode to AM335x EVM
      1. 6.2.1 Patch Description
    3. 6.3 WoWLAN (Wake on WLAN) Mode Enable Procedure
      1. 6.3.1 Commands and Expected Output
      2. 6.3.2 Rx Filter Configuration
        1. 6.3.2.1 Rx Filter Configuration Examples
    4. 6.4 WoWLAN - Magic Packet
    5. 6.5 Block Acknowledgement (BA) Filter Setting
    6. 6.6 Hardware Modification Engineering Change Order (ECO) Request for AM335x EVM
  8. WiLink8 Suspend Resume Mode
    1. 7.1 Suspend Resume Example With AM437x SDK
  9. Access Point (AP) Dynamic Frequency Selection (DFS) Master Support
    1. 8.1 Setup and Configuration
    2. 8.2 User Guide & Examples
    3. 8.3 Errata/Limitations
  10. Station Mode - Alternative Method, With iw Commands, Explained
    1. 9.1 Step 1- Check if the wlan0 Interface is Already Running
    2. 9.2 Step 2- Bringup wlan0 Interface if Not Running
    3. 9.3 Step 3 - Connect Device to Available Acces Point
  11. 10References

WoWLAN - Magic Packet

The magic packet is a broadcast frame containing anywhere within its payload 6 bytes of all 255 (FF FF FF FF FF FF in hexadecimal), followed by sixteen repetitions of the target computer's 48-bit MAC address, for a total of 102 bytes.

Since the magic packet is only scanned for the string above, and not actually parsed by a full protocol stack, it may be sent as any network and transport-layer protocol, although it is typically sent as a UDP datagram to port 7 or 9, or directly over Ethernet as EtherType 0x0842.

The wl18xx firmware does not support scanning of the entire Ethernet frame for the magic packet. Besides, as mentioned before, the max size of a pattern is 81 bytes.

However, it is possible to define patterns that can dissect an actual implementation of the magic packet by comparing a subset of the actual magic packet. An example is shown below:

Wakeup on magic packet with EtherType = 0x0842 or UDP port no: 9

iw phy0 wowlan enable patterns 01:02:03:04:05:06:-:-:-:-:-:-:08:00:45:-:-:-:-:-:-:-:-:11:-:-:-:-:-:-:C0:A8:01:04:-:-:00:09:-:-:-:-:ff:ff:ff:ff:ff:ff:01:02:03:04:05:06:01:02:03:04:05:06 01:02:03:04:05:06:-:-:-:-:-:-:08:42:ff:ff:ff:ff:ff:ff:01:02:03:04:05:06:01:02:03:04:05:06 

Where,

01:02:03:04:05:06 -> Destination MAC ID C0:A8:01:04 -> Destination IP address (192.168.1.4)

The utilities "etherwake" or "wakeonlan" (on Linux) or "Wol Wake on Lan Wan" (Android) can be used to wake up the WL18xx host after setting the above pattern.

Command to run on the remote (Ubuntu) machine:

# etherwake -iwlan2 -D 01:02:03:04:05:06 
OR
# wakeonlan -i 192.168.1.4 01:02:03:04:05:06