WiLink8 devices can support two
virtual APs on the same physical device. The two virtual APs operates on the same RF
channel. In mBSSID mode, the WLAN Component will create two SoftAP network
interfaces.
- Each AP will have a separate
BSSID and SSID.
- Each AP will transmit a separate
Beacon.
- Each virtual AP will respond to
Probe-Requests separately.
- Support up to 10 traffic links
(10 connected STAs) total, for both BSSs combined.
- WiFi Privacy / Encryption
- Each of the two APs will
be able to enable or disable Privacy, regardless of the other AP’s
setting.
- All combinations of
Encryption types will be supported.