SWRU587A November 2021 – March 2023 AWR2944
This text box prompts users to select the desired RCS for getting the Maximum Range at which an object of this RCS is likely to be detected, based on the scene and object detection parameters selected on the left-hand side. Hints for approximate values follow:
The value for Maximum Range calculated based on this input is shown in the Maximum Range for desired RCS (m) display box.