This document provides information about CC33xx family of devices and Wi-Fi® features, as well as TI proprietary enhancements. The document does not provide the complete application programming interface (API) set, but a high-level overview of the features. The CC33xx Linux® software package is based on the open source mac802.11 implementation; the complete API can be found in: https://elixir.bootlin.com/linux/latest/source/net/mac80211.
Wi-Fi® is a registered trademark of Wi-Fi Alliance.
Linux® is a registered trademark of Linus Torvalds in the U.S. and other countries.
All trademarks are the property of their respective owners.