SWRU616B September 2023 – April 2024 CC3300 , CC3301 , CC3301MOD , CC3350 , CC3351
Frame aggregation reduces overhead of the 802.11 protocol and increases data throughput by using a single PHY or MAC header to send multiple frames of data. There are primarily two methods available to accomplish frame aggregation: aggregate MAC service data unit (A-MSDU) and aggregate MAC protocol data unit (A-MPDU).
The main distinction between MSDU and MPDU is how information transmitted through the respective layers.
Beyond the difference in transmission between layers, there is also a difference in the frame structure when the units are aggregated.
In frame aggregation these techniques are combined so that multiple MSDUs can be concatenated into a single MPDU and transmitted. These aggregate exchange sequences are implemented through a protocol that acknowledges (ACKs) multiple MPDUs with a single block ACK. For more information on block ACK sessions, see Section 2.3. The CC33x can both transmit and receive data in the A-MPDU format and is able to receive data in the A-MSDU format.