SWRU616B September 2023 – April 2024 CC3300 , CC3301 , CC3350 , CC3351
In the Bluetooth Low Energy provisioning mode, the Bluetooth Low Energy role is active and the user can connect to the CC33xx device via bluetooth. Once connected, the user can send the necessary credentials over and then the device can utilize STA mode to connect to the desired AP. A benefit CC33xx device is that it can have Bluetooth Low Energy and STA mode active simultaneously.