SWRU616B September 2023 – April 2024 CC3300 , CC3301 , CC3301MOD , CC3350 , CC3351
The CC33xx supports the following three authentication types: open, personal and enterprise. However, which types are supported depends on what mode the CC33xx is in.
The first authentication type is open, which refers to APs that do not require a password to join.
The second is personal authentication, where the password is configured to the AP and the AP itself authenticates the peer device using a password. The supported personal authentication types are:
The third is enterprise authentication (supported in STA Mode), where a RADIUS (Remote Authentication Dial-In Service) server behind the AP authenticates the peer device. The following list the supported enterprise authentication types: