SWRU622 August 2024 AWRL1432 , AWRL6432 , IWRL1432 , IWRL6432 , IWRL6432AOP
External watchdog timer can be used to monitor the mmWave radar device for detecting the software codes (Application code, driver code, and so forth) from entering the lockup state or increase in implementation time. The external watchdog timer can be serviced from the GPIO's of the mmWave radar device. If the external watchdog timer is not serviced regularly as expected then the timer can trigger the NRESET signal to the device. On reset from external watchdog timer, mmWave radar device would provide a clean restart of the device and reload the flash contents from FLASH memory. One of the examples for the external watchdog timer is TPS3430 - Automotive Window Watchdog Timer with Programmable Reset Delay. The watchdog timer can also be used to detect and recover from a hardware fault.