SWRU622 August 2024 AWRL1432 , AWRL6432 , IWRL1432 , IWRL6432 , IWRL6432AOP
A watchdog timer module is available on the xWRLx432 device. A watchdog timer can act as a last method of defense against runaway code or infinitely looping code. This can prevent the device from entering an unknown state and can result in unknown power draw or loss of communication within a larger system.
The WDT does not provide coverage when the device is in low power/deep sleep mode
The internal watchdog is not meant to cover all failure modes on the device, which includes but is not limited to random bit flips or transient faults. An appropriate functional safety assessment must be taken by the system integrator to determine if the internal watchdog is sufficient for the use-case.