SWRU622 August 2024 AWRL1432 , AWRL6432 , IWRL1432 , IWRL6432 , IWRL6432AOP
This document details how to utilize the ROM Bootloader(RBL) in a variety of different use-cases and resolve issues that may arise from using the RBL in these scenarios. In addition, due to the rigidity of the RBL (as it is programmed into the device ROM), this document also introduces the secondary bootloader(SBL), which provides greater flexibility in what can be loaded onto the device (primary and secondary image or multiple unique user applications) and how it can be loaded (via any serial streaming interface). Lastly this document covers reset behavior, with a focus on warm reset behavior on the xWRLx432 and considerations to be made in user application design and hardware design.
This document provides a better understanding of how the application software interacts with the RBL/SBL and how it can leverage the RBL and SBL for varying levels of host-control during booting and reset procedures. Complete implementation details on the RBL and the SBL can be found in the xWRLx432 TRM.
Above is an overview of the initialization process and is detailed below:
Once the device is in functional mode, the RBL ensures that the application image is properly transferred over to RAM and hands control of the device to the user application. If this flow is interrupted by any common failure, the device goes into a safe state and will not boot the user application.