SWRU622A August 2024 – September 2024 AWRL1432 , AWRL6432 , IWRL1432 , IWRL6432 , IWRL6432AOP
The target binary file is composed of the following sections:
The MMWAVE-L-SDK package for the xWRLx432 device from TI includes the MulticoreImageGen utility, which constructs the complete image with the previously listed components. See Boot Image Format under Device Initialization in the TRM for more information on the structure of the application image