SWRU624A April   2024  – July 2024 CC3301

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Download Prerequisites
  5. 2Build Prequisites
  6. 3Patch Steps
    1. 3.1 Additional Steps
    2. 3.2 Overall Steps
  7. 4Check the Applied Patch
  8. 5Build Steps
  9. 6Using the Built App File
  10. 7Revision History

Overall Steps

The remainder of the steps should be executed whether the source code came from Git or a compressed file:

  1. If you have not done so already, download the TI-Wi-FiQuickTrack-ControlAppC-Patcher installer linked in the download prerequisites.
    1. Confirm that the installer is compatible with the OS being used (Windows or Linux)
    2. Note: if the Linux installer was used it will need to be converted into an executable using the chmod +x command
  2. When you run the installer make sure to update the Installation Directory to Wi-FiQuickTrack-ControlAppC source files directory that was downloaded previously either through Git clone or from the zip/tar file (see previous steps).
    1. Path of the given directory should contain source files such as .c and .h files and a Makefile