SWRU624 April 2024 CC3301
The QuickTrack Control App is a Wi-Fi automation test tool utilized for Wi-FiĀ® Certification. This User Guide is intended to provide an overview of using the QuickTrack Control App with CC33xx devices to certify end products. The required software and set-up steps vary slightly between Linux and Windows operating softwares.
Please note that Git Bash for Windows must be downloaded at the following link when using a Windows operating system: https://git-scm.com/download/win
The source files required to build and use the QuickTrack Control App can be cloned or downloaded and extracted from GitHub. It is imperative that the tags and checkouts are verified to ensure that the correct version is downloaded.
After using one of the above options to acquire the source file, the installer specific to the operating system being used must be downloaded. Both installers can be found at on the external TI Drive, the links and access codes are included below.