SWRU624A April 2024 – July 2024 CC3301 , CC3301MOD
To use the QuickTrack Application provided by the WFA it is necessary to refer to WFA provided documentation. To do so a membership with the WFA is needed which provides access to the QuickTrack Test Tool User Manual that outlines how to download and use the QuickTrack application. Once those steps have been completed, continue with the steps below to test the DUT.
Note as mentioned previously, in the example provided by this document the DUT is an AM335x host with a CC33xx boosterpack.
Confirm that the certificates are located at /etc/default/certificates and that the same path is updated in the tool settings to match:
date -s '2023-11-23 14:34:00'
cd /etc/wpa_supplicant/
./app -i wlan0 -p 9004 &
cd /usr/share/cc33xx
./sta_start.sh
cd /etc/wpa_supplicant/
./app -i wlan1 -p 9004 &
cd /usr/share/cc33xx
./ap_start.sh
For more information on QuickTrack specifics it is recommended to refer to the support documentation provided by the WFA to WFA members on the website. The QuickTrack Test Tool Getting Started Guide provides a high level overview and list of resources and installations, while the QuickTrack Test Tool User Manual goes into further detail on many of the steps (these documents are available on the wfa website: https://www.wi-fi.org/). Additionally TI is available for additional support on E2E.