SWRU629 September 2024
The LP-EM-CC35X1 features 2 x 20 pin connectors that provide access to many of the CC35xxE pins and features. The LaunchPad header pinout is standard in TI, allowing easy stacking of other TI BoosterPacks on the LP-EM-CC35xx for quick interface with peripheral boards.
The CC35xxE LaunchPad follows this standard. For CC35xxE pin-mapping assignments and functions, see Figure 2-19.
All the signals are referred to by the GPIOx in the SDK. The default mappings are shown in Figure 2-19. Some of the pins are repeated across the connector. For example, GPIO4 is available on header pin 25 and pin 39, but only pin 25 is connected by default. The signal on LaunchPad header pin 39 is marked with an asterisk (*) to signify that the signal is not connected by default. The signal can be routed to the pin by using a 0Ω resistor in the path.