SWRU631 November 2024
By default, the board is designed to be used with the DP83867E PHY with the RJ45 connector. To enable the DP83TG720S-Q1 PHY with the MATEnet connector, the following hardware changes must be made. For help with locating these components on the PCB, refer to the provided Schematic, BOM, and assembly files.
The automotive Ethernet PHY (U4) and port (J4) on the AWR2E44PEVM have not been tested by Texas Instruments to be compliant with any regional standards such as Radio Equipment Directive 2014/53/EU. If the user wishes to populate the components necessary to utilize this port, it is up to the user to do any necessary testing to ensure that the port is compliant with all applicable regional standards before use. Any modifications done to enable the J4 port will invalidate the existing RED 2014/53/EU certification of the AWR2E44PEVM.