SWRZ102C November 2021 – December 2024 AWR2944
PRODUCTION DATA
Incorrect behavior seen when context switch happens in the last parameter-set in the Hardware Accelerator (HWA 2.1)
AWR294`x ES2.0
At the end of the last parameter-set of the last loop in low-priority context, if a context-switch happens to high priority, then an incorrect behavior is observed when returning back to low-priority. This incorrect behavior can manifest itself as a fresh (unintended) re-start of the low-priority loop once completed. Following are the erroneous conditions:
It is recommended to not enable context switch in the last parameter-set of the above mentioned conditions. In case, the last parameter-set has to have context switch enabled, user could add a dummy parameter-set with context switch disabled as the last parameter-set.