SWRZ115B March 2021 – May 2024 AWR1843AOP
Surface Wave Artifact from PCB
AWR1843AOP ES1.0
Large PCBs area around the E-plane causes surface waves that create large ripples in the elevation direction of the AoP antenna radiation pattern.
Workaround #1:
Keep the Edge of PCB close to the edge of the AoP device in the E-plane to minimize the surface wave ripples.
or
Workaround #2:
If a larger board is needed for the solution, a trapezoid cutout with the PCB edge less than <0.3mm from the edge of the AoP should be implemented to minimize the ripples caused by surface waves.