Figure 2-1 and Table 2-1 describe package symbolization and the device revision code.
Figure 2-1 Package Symbolization
Table 2-1 Revision IdentificationDEVICE REVISION CODE | SILICON REVISION |
---|
F | PG3.0 |
The die markings do not indicate the silicon revision. However, customers can determine the silicon revision by one of the following methods:
- TI provided software functions
in chipinfo.c:
- HwRevision_t ChipInfo_GetHwRevision( void )
- Returns: chip HW revision
- HWREV_2_2 is returned for CC2652PSIP revision
F.
- SmartRF™ Studio:
- When connecting to a
CC2652PSIP device, the version number is shown in the lower-left corner
(see Figure 2-2).
- Package label:
- The die revision name is shown on the tape and reel label as shown in the example label in Figure 2-3.
- Entry (2P) lists the revision F.