TIDA029A july 2019 – june 2023 CC2640R2F-Q1 , CC2642R , CC2642R-Q1
The PCB + RF absorbing material + tin-plated copper foil + metal hardware setup is the only hardware setup that the offset was not adjusted for AoA to equal zero when Phi equals 0. The results are not linear for the whole –90° to 90° range and to balance the error across the full angle range, the offset was set to have an error of 7° when Phi equals 0. Better compensation methods can be used to improve the results but in this paper, only basic best fit line linear compensation was implemented. Table 4-3 shows the gain and offset used for each frequency.
Frequency (MHz) | Channel | Gain | Offset |
---|---|---|---|
2402 | 37 | 2.44 | –2.55 |
2404 | 0 | 2.44 | –2.12 |
2406 | 1 | 2.44 | –2.87 |
2408 | 2 | 2.44 | –3.07 |
2410 | 3 | 2.44 | –3.16 |
2412 | 4 | 2.44 | –3.28 |
2414 | 5 | 2.44 | –3.22 |
2416 | 6 | 2.38 | –2.71 |
2418 | 7 | 2.38 | –2.92 |
2420 | 8 | 2.38 | –2.92 |
2422 | 9 | 2.38 | –2.21 |
2424 | 10 | 2.38 | –3.15 |
2426 | 38 | 2.38 | –2.55 |
2428 | 11 | 2.38 | –2.68 |
2430 | 12 | 2.38 | –3.11 |
2432 | 13 | 2.38 | –2.82 |
2434 | 14 | 2.38 | –2.74 |
2436 | 15 | 2.38 | –2.74 |
2438 | 16 | 2.38 | –2.66 |
2440 | 17 | 2.38 | –2.44 |
2442 | 18 | 2.38 | –2.37 |
2444 | 19 | 2.44 | –2.65 |
2446 | 20 | 2.44 | –2.37 |
2448 | 21 | 2.44 | –2.62 |
2450 | 22 | 2.44 | –2.5 |
2452 | 23 | 2.5 | –2.68 |
2454 | 24 | 2.5 | –2.35 |
2456 | 25 | 2.5 | –2.4 |
2458 | 26 | 2.5 | –2.62 |
2460 | 27 | 2.56 | –2.4 |
2462 | 28 | 2.56 | –2.33 |
2464 | 29 | 2.56 | –2.53 |
2466 | 30 | 2.63 | –2.66 |
2468 | 31 | 2.63 | –2.32 |
2470 | 32 | 2.7 | –2.37 |
2472 | 33 | 2.7 | –2.93 |
2474 | 34 | 2.7 | –2.72 |
2476 | 35 | 2.7 | –2.3 |
2478 | 36 | 2.7 | –2.3 |
2480 | 39 | 2.7 | –2.43 |
Figure 4-22 and Figure 4-23 show the difference in the uncompensated and compensated error.
The error is greatly improved with compensation. Depending on the frequency, this hardware setup shows less than 10° of error from –90° to 40° and 70° to 90°. There is considerable error from 40° to 65° for most frequencies. Better compensation methods could greatly improve this error while still maintaining the full range of ±90°. Figure 4-24 and Figure 4-25 show the uncompensated AoA vs compensated AoA.