TIDA029A july   2019  – june 2023 CC2640R2F-Q1 , CC2642R , CC2642R-Q1

 

  1.   1
  2.   Bluetooth Angle of Arrival (AoA) Antenna Design
  3.   Trademarks
  4. 1Introduction
  5. 2Angle of Arrival Antenna Design Considerations
    1. 2.1 Antenna Spacing
    2. 2.2 RF Switch Considerations
  6. 3Dipole Antenna Array
    1. 3.1 Dipole Antenna Strengths and Weaknesses
    2. 3.2 Angle Measurement Plane
    3. 3.3 PCB Implementation
    4. 3.4 Two Dipole Array Test Results
      1. 3.4.1 Total Radiated Power (TRP)
      2. 3.4.2 Measuring Antenna 1 and 2 Phase Difference
        1. 3.4.2.1 Bare PCB
        2. 3.4.2.2 PCB + RF Absorbing Material
        3. 3.4.2.3 PCB + RF Absorbing Material + Tin-Plated Copper Foil
        4. 3.4.2.4 PCB + RF Absorbing Material + Tin-Plated Copper Foil + Metal
      3. 3.4.3 Phase Difference vs Distance
  7. 4Calculating AoA From IQ Measurements
    1. 4.1 Dipole Antenna Array Uncompensated Angle of Arrival Results
      1. 4.1.1 Bare PCB Uncompensated AoA
      2. 4.1.2 PCB + RF Absorbing Material Uncompensated AoA
      3. 4.1.3 PCB + RF Absorbing Material + Tin-Plated Copper Foil Uncompensated AoA
      4. 4.1.4 PCB + RF Absorbing Material + Tin-Plated Copper Foil + Metal Uncompensated AoA
    2. 4.2 Dipole Antenna Array Compensated AoA Results
      1. 4.2.1 Bare PCB AoA With Compensation
      2. 4.2.2 PCB + RF Absorbing Material + Tin-Plated Copper Foil Compensated AoA
      3. 4.2.3 PCB + RF Absorbing Material + Tin-Plated Copper Foil + Metal Compensated AoA
      4. 4.2.4 Hardware Setup Compensated Results Comparison
  8. 5References
  9. 6Revision History

Dipole Antenna Array Compensated AoA Results

In this section, gain and offset compensation is added to the base calculated AoA values in Section 4.1 (excluding the PCB + RF absorbing material hardware setup) to reduce the AoA error from the actual angle Phi. The compensation is applied as Equation 5 shows.

Equation 5. GUID-78D7EAE0-BA96-40E0-BFDD-6123FEDCFBF0-low.gif

where

  • θ equals the calculated AoA
  • b equals the offset
  • m equals the gain

For all hardware setups except the setup with the metal stand, the offset value was selected to make sure that when Phi equals zero, the calculated average AoA also equals zero. This offset was adjusted for each individual frequency as all frequencies require a slightly different offset value. To calculate the gain, the best fit line method was used for each frequency in the most linear range ( that is, –65° to 65°) after adding the required offset. However, there is much smaller variance of gain values over frequency as the majority of frequencies require the same gain or similar gain values.