TIDA029A july 2019 – june 2023 CC2640R2F-Q1 , CC2642R , CC2642R-Q1
All radiation measurements are done on a TIDA-01632 PCB without any absorbing material or copper foil attached. The CC2640R2F-Q1 device on the TIDA-01632 is configured to output a constant wave at 2440 MHz with 0 dBm. The measured total radiated power (TRP) is –8.71 dBm and –8.97 dBm giving an antenna efficiency of around 14% (0.3 dB loss in the RF switch - SKYA21001). In the following measurements, the z-axis is perpendicular to the PCB, with the x-axis as the height and the y-axis as the length shown in Figure 3-16.
In the total radiated power plots, Theta represents the rotation of the PCB from the z-axis to the y-axis (turntable base rotating) and Phi represents the z-axis to the x-axis (rotating the arm from Figure 3-14).
The TRP was also measured with the TIDA-01632 PCB mounted on a metal stand with RF absorbing material (WaveX WX-A-010-12P) and tin plated copper foil (3M 1183) attached between the PCB and the metal stand shown in Figure 3-31. The added metal around the antenna drastically degrades the efficiency but ensures that no RF signals are received from the back side of the PCB. A measured TRP of around –23 dBm indicates an antenna efficiency of just 0.5%.