TIDT224 March 2021
The following image shows the FET switch node voltage SW (Red) at TP4. The input voltage is 12 VDC and both 15-V outputs are loaded to 100 mA.
The following image shows the FET switch node voltage SW (Red) at TP4. The input voltage is 12 VDC and both 15-V outputs are loaded to 50 mA.
The following image shows the FET switch node voltage SW (Red) at TP4. The input voltage is 12 VDC and both 15-V outputs are loaded to 10 mA.
The following image shows the FET switch node voltage SW (Red) at TP4. The input voltage is 15 VDC and both 15-V outputs are loaded to 100 mA.
The following image shows the FET switch node voltage SW (Red) at TP4. The input voltage is 15 VDC and both 15-V outputs are loaded to 50 mA.
The following image shows the FET switch node voltage SW (Red) at TP4. The input voltage is 15 VDC and both 15-V outputs are loaded to 10 mA.
The following image shows the secondary winding voltage of the transformer at T1- pin 5 (Red) with respect to T1 – pin 6. The input voltage is 15 VDC and both 15-V outputs are loaded to 100 mA.
The following image shows the secondary winding voltage of the transformer at T1- pin 5 (Red) with respect to T1 – pin 6. The input voltage is 15 VDC and both 15-V outputs are loaded to 50 mA.