TIDT239A April 2021 – July 2021
The output voltage during USB Type-C voltage transitions are shown in the following images. The input was 115 VAC, 60 Hz and the output was unloaded. This behavior is not dependent on input voltage.