TIDT283 May 2022
Output ripple waveforms are shown in the following figures.
The green waveform in Figure 2-2 shows the VEE-COM rail ripple while the output is switching a 100-nF capacitive load at 1 kHz. The peak-to-peak ripple is 252 mV, which is 6.3%.
The green waveform in Figure 2-3 shows the VEE-VDD rail ripple while the output is switching a 100-nF capacitive load at 1 kHz. The peak to peak ripple is 865 mV, which is 3.9%.
The green waveform in Figure 2-4 shows the VEE-COM rail ripple while the output is switching a 100-nF capacitive load at 35 kHz. The peak to peak ripple is 232 mV, which is 5.8%.
The green waveform in Figure 2-5 shows the VEE-VDD rail ripple while the output is switching a 100-nF capacitive load at 35 kHz. The peak to peak ripple is 800 mV, which is 3.6%.