In this lab, the voltage loop Gv , is closed with a electrical load (constant current mode) at the output.
- Run the project by clicking the Resume button in the Tool Bar
- Set the load current below 2 A during start up
- Increase the input VSEC DC voltage from 0 V to 48 V
- Clear the trip by writing "1" to the CLLLC_start variable in the watch window as shown in Figure 1-4, this closes the voltage loop and the converter performs soft-start until the output voltage ramps up to 400 V
- Test the close loop operation by varying "CLLC_vSecRef_Volts " in the watch window