• Menu
  • Product
  • Email
  • PDF
  • Order now
  • AM437x Single-Chip Motor-Control Design Guide

    • TIDU800B March   2015  – December 2018

       

  • CONTENTS
  • SEARCH
  • AM437x Single-Chip Motor-Control Design Guide
  1.   A
    1.     A.1 Field Oriented Control (FOC)
    2.     A.2 Position and Speed Motor Control
  2.   Revision History B
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

DESIGN GUIDE

AM437x Single-Chip Motor-Control Design Guide

A

A.1 Field Oriented Control (FOC)

The FOC attempts to separately control the torque-producing and magnetizing flux components of the stator current. By decoupling control of the magnetization, the torque producing component of the stator flux becomes an independent torque control. To decouple the torque and flux, several mathematical transforms must be implemented. The FOC consists of controlling the stator currents represented by a vector. This control is based on projections which transforms a three-phase time- and speed-dependent system into a two co-ordinate (d and q co-ordinates) time-invariant system. Field-orientated controlled machines need two constants as input references: the torque component (aligned with the q co-ordinate) and the flux component (aligned with d co-ordinate).

The first set of inputs to FOC are the motor phase currents. These measurements feed the Clarke transformation module. The outputs of this projection are designated Isα and Isβ. These two components of the current are the inputs of the Park transformation that gives the current in the d,q rotating reference frame. The Isd and Isq components are compared to the references Isd* (the flux reference) and Isq* (the torque reference). This control structure can control either PMSM or HVPM machines by changing the flux reference and obtaining rotor flux position. When controlling a PMSM, Isd* is set to zero. The torque command Isq* is the output of the speed regulator. The outputs of the current regulators are Vsd * and Vsq *. These are the inputs to the inverse Park transformation. The outputs of this transformation are Vsα * and Vsβ *, which are the components of the stator vector voltage in the α and β stationary orthogonal reference frame. These are the inputs of the Space Vector PWM. The outputs of the Space Vector PWM block are the signals that drive the inverter.

Both Park and inverse Park transformations need the rotor flux position. In a synchronous machine, the rotor speed is equal to the rotor flux speed. This is calculated from the rotor position of the QEP encoder. The rotor flux position (θ) is directly measured by position sensor or by integration of rotor speed. The rotor position permits the variable transformation from a stationary reference frame to a synchronously-rotating reference frame. As a result of the Park transformation, the q-axis current will control torque while d-axis current is forced to zero. The torque and flux decouple from each other. To view the overall block diagram of this project, see Figure 14.

TIDEP0025 BD_Sensored_Field_Oriented_Ctrl_TIDU800.gifFigure 14. Block Diagram of Sensored Field Oriented Control

A.2 Position and Speed Motor Control

To view a diagram of the speed and position FOC loop for a PMSM, see Figure 15. By reducing the system components and increasing efficiency, the AM437x family enables cost-effective integrated designs of a communications system and intelligent controllers for three-phase motors. The FOC algorithm maintains efficiency across a wide range of speeds while using a space vector modulation technique to compensate for the sinusoidal-voltage waveform applied to the motor by controlling the flux from the rotor coordinates. This approach produces a minimum amount of torque ripple when driving a sinusoidal BEMF motor with sinusoidal currents.

In LEVEL4 the controlling variables are lsw and speed.

TIDEP0025 Level_4_Speed_Closed_Field_Oriented_Ctrl_TIDU800.gifFigure 15. LEVEL4 - Speed Closed Field Oriented Control Loop

In LEVEL5, the controlling variables are lsw and angle.

TIDEP0025 Level_5_Position_Closed_Field_Oriented_Ctrl_TIDU800.gifFigure 16. LEVEL5 - Position Closed Field Oriented Control Loop

LEVEL6 is a combination of LEVEL4 and LEVEL5. In Level 6, the control variables are msw, lsw, speed, and angle.

TIDEP0025 Shot_FOC_Motor_Ctrl_Lvl_6_UI_TIDU800.pngFigure 17. FOC Motor Control Level 6

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale