TIDUAY6E
November 2015 – March 2020
Revision History
4.1.2.3.2.1
Setting Software Options for Build 2
Make sure the hardware is set up as outlined in the previous sections (see
Figure 16
). Do not supply any high-voltage power yet to the board.
powerSUITE settings: On the powerSUITE page select under "Project Options" section:
"Closed Current Loop" for the build level
"DC" for the output
Either "SDFM" or "ADC" for sensing method depending on what is on the design (On this design, both SDFM and ADC sensing methods are present).
Save the page.
Under "Control Loop Design", select Tuning → Current Loop, Comp Number → COMPI, Comp Style → DCL_PI_C3, and click on the Compensation Designer icon.