TIDUBE1D January 2016 – August 2024
The MOSFET switch is driven by a gate output that is clamped at 15.2V internally for VCC bias voltages greater than 15.2V. An external gate drive resistor is recommended to limit the rise time and to dampen any ringing caused by the parasitic inductance and capacitance of the gate drive circuit. This resistor also helps by meeting any EMI requirements of the converter. This design uses a 22Ω resistor; the final value of any design depends on the parasitic elements associated with the layout of the design. To facilitate a fast turnoff, place a standard 100V, 1A Schottky diode or switching diode anti-parallel with the gate drive resistor. A 10kΩ resistor is placed between the gate of the MOSFET and ground to discharge the gate capacitance and protect from inadvertent dV/dT triggered activations.
The maximum voltage across the FET is the maximum output boost voltage (that is, 425V), which is the overvoltage set point of the PFC converter used to shut down the output. Considering a voltage de-rating of 30%, the voltage rating of the MOSFET must be greater than 550V DC.
This design uses an IPW60R099P6 MOSFET of 600V with 37.9A at 25°C and 24A at 100°C. If cost is a concern, this design also can use an IGBT to replace the MOSFET. This design needs a heat sink of the appropriate size for the MOSFET or IGBT.