TIDUBF0 January 2022
Because this reference design is targeted at automotive applications, there are several considerations that limit design choices. Additionally, the following list of system-level specifications helped shape the final overall design:
Before parts are chosen, the input voltage range, required voltage rails, and required current per rail must be known. In this case, the input voltage is a pre-regulated 9-V supply coming in over the coaxial cable. This system has only two main devices, the imager and serializer, which are responsible for power consumption during operation. Table 2-1 shows the requirements of the supplies:
PARAMETER | VOLTAGE (V) | CURRENT (mA) | POWER (mW) |
---|---|---|---|
DS90UB933 | |||
VDD | 1.8 | 98 | 176 |
OX01F10 | |||
VDD-D | 1.1 | 170 | 187 |
VDD-IO | 1.8 | 21 | 38 |
VDD-A | 3.3 | 33 | 109 |
Oscillator | |||
VDD | 1.8 | 3 | 5 |
Total | |||
VDD-D | 1.1 | 170 | 187 |
VDD-IO | 1.8 | 122 | 220 |
VDD-A | 3.3 | 33 | 109 |
The9-V supply over the coaxial cable is first stepped down to 3.8 V, which then supplies the rest of the system on the camera module. In this design, the 1.8-V rail supplies both the DS90UB933 supply, and the interface supply of the OX01F10 imager. The OX01F10 3.3-V analog rail requires 33 mA, the DS90UB933 serializer 1.8-V rail requires 98 mA, and the OX01F10 digital 1.1-V rail requires 170 mA.
Assuming 85% efficiency to simplify calculations with the previous values, it is calculated that the 3.8-V supply will require 160 mA to successfully power the 1.1-V, 1.8-V, and 3.3-V rails. Because the input and output voltages, output current requirements, and total wattage consumption are known, calculate the input current using Equation 5:
This information provides a strong foundation in the selection of power topologies and inductive passives that are explained in later sections.
Due to the requirement of Q100, it is mandatory that the switching frequency is rated outside of the AM band and must satisfy the voltage and current requirements derived previously. As the input voltage is a regulated voltage that will always be greater than any of the power rails produced, the power topologies selected should either be step-down converters (bucks) or LDOs. Bucks are generally included in supplies where switching noise is not a significant concern, and power savings is the largest care about. Conversely, LDOs can be incorporated in establishing low-noise analog supplies that reduce inherent noise and are more robust against EMI interactions; however, this is at the expense of larger current consumption.
In this design, a single Power Management IC is responsible for powering the supply rails. This device, the TPS650320-Q1, was chosen as it incorporates three step-down converters (BUCKS) and an LDO in a single 4.0-mm x 4.0-mm VQFN package. The current requirements of the design also played an important role in the selection of the device, as the secondary BUCKS are capable of providing 600 mA, while the LDO is capable of supplying a maximum current output of 300 mA. BUCK1 steps down the 9-V POC input to 3.8 V. The 3.8-V rail then supplies power to BUCK2, BUCK3, and the LDO input. BUCK 2 provides the interface and digital supply for both the OX01F10 imager and DS90UB933 serializer, while the LDO output creates a clean, low-noise supply for the 3.3-V analog supply for the OX01F10.