TIDUBF0 January 2022
Figure 3-2 shows the setup to test the camera module reference design. This design includes an OX01F10 image sensor, which connects to the DS90UB933-Q1 serializer over CSI-2 and I2C interfaces. The DS90UB933-Q1 serializer then connects through POC to a DS90UB954-Q1 deserializer. Note that for test setup, only one channel is used from the DS90UB954-Q1 device. The Analog LaunchPad™ GUI writes all the back channel I2C setting configurations for the IMX390, DS90UB933-Q1, and DS90UB954-Q1 devices.