TIDUBF0 January 2022
I2C communication between the DS90UB954-Q1 EVM and OX01F10 imager over the FPD-Link III back channel can be confirmed with the Analog LaunchPad GUI. Figure 3-10 and Figure 3-11 show the established link with the serializer on RX port 1, and the corresponding register map.
Read and writes to the imager, at slave alias address 0x6C (7-bit), are confirmed with the built-in Python scripting window of the Analog LaunchPad. Register 0x3035 reads data 0x6C, which is the expected default value for the register.