TIDUBF0 January 2022
Once the FPD-Link III setup is done for the DS90UB933-Q1 and DS90UB954-Q1 devices, the I2C initialization can now be done on the OX01F10. For these writes, see the OX01F10 data sheet for register settings. There are many register settings listed to configure both the imager and ISP, but as long as the DS90UB933-Q1 and DS90UB954-Q1 FPD-Link III parts are configured, the I2C back channel allows for the OX01F10 to be accessed at address 0x6C. For this testing, the OX01F10 is configured for YUV422 DVP output at 1340 × 1020 resolution.